Tool/software:
Hello teams.
Please tell me about below questions.
Q1. If a signal exceeding the IO rating is applied to either IN1 or IN2, is there a possibility that both S30 and S31 will short to GND?
(The board is designed with S30 = 3.3V: high, S31 = GND: low)
Q2. If an overvoltage is applied to S30 (fixed high), is it possible that S31 will also short to GND?
(The board is designed with S30 = 3.3V: high, S31 = GND: low)
Best regards,
Akashi