Part Number: DS90UB960-Q1
Other Parts Discussed in Thread: DS90UB953-Q1
Tool/software:
Hi,
We are using the DS90UB960-Q1 deserializer and DS90UB953-Q1 serializer to transfer the MIPI data. We need to generate a 10 Hz FrameSync signal with a 10% duty cycle from the deserializer.
We referred to the deserializer datasheet for FrameSync generation.
Calculation for the 10 Hz frequency: (1 sec / 10 Hz) / 600 ns - total count - approximately 166,667.
For a 10% duty cycle, the high time is 16,666, and the low time is 150,000.
Is it possible to generate 10 Hz at a 10% duty cycle?