Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Tool/software:
Good day
I have 2 questions which is not clear to me from the datasheet.
1) Can I configure the Phy only using the registers? If I make changes in the registers, when are those changes valid. Do I need to reset the chip?
Can I dynamically change between using Fiber or Copper?
2) If I supply 3.3V and the 2.5V DC,Do I also need to supply the 1.0 and 1.8V.