Part Number: TMUXHS4412
Tool/software:
on spec of TMUXHS4412, I found 3 AC couple cap placement option as Figure7-1
in my board, no connector, all devices are on the same board, and the endpoint is very close to TMUXHS4412.
To save the space and minus the cap qty, i want to change place of the endpoint ac couple cap as attached pic. From Endpoint TX side to TMUXHS4412 TX side. Pls confirm if it is OK.

2nd question.
The TMUXHS4412 can tolerate polarity inversions for all differential signals on Ports D, DA, and DB. In such flexible implementation, users must ensure that the same polarity is maintained on Port D versus Ports DA/DB.
if the PCIE host and endpoint support polarity inversions.
Below strucure should be OK, pls help to confirm, thanks.