Part Number: MAX202
Other Parts Discussed in Thread: TRS202E, MAX232E, MAX3232, TRSF3232E, TRS3232, MAX3232E
Tool/software:
Hi team,
Do we have new gen of MAX202? or do we have similar spec recommendation?
Thanks
Lilian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lilian,
Is there a particular feature set or improvement you are looking for? Faster data rate, improved ESD protection, wider VCC supply range, auto-powerdown features?
Typically I recommend MAX3232E which supports either a 3.3V or 5V supply, 15kV IEC ESD protection, and 250kbps. It also has SOIC and TSSOP packages comparable to MAX202. Note MAX3232E has 15kV HBM and IEC protection, while MAX202 only has 15kV HBM. Having 15kV IEC protection typically means external ESD diodes are no longer necessary.
Regards,
Ethan