Part Number: DS110DF111
Tool/software:
I have a custom a PCB design that involves the DS110DF111 to interface between a processor to Cisco optical switch. I'm currently testing with Cisco Compatible Duplex 10GBASE-ZR/ZW Ethernet 10G Ethernet / 8G FC SFP+ transceivers designed for long distance optical communications up to 80 km with signaling rates up to 10.3125 Gbps, which are connected via optical patch cables between custom PCB SFP+ ports to the SFP+ ports on the switch.
Currently, the Signal is not detected and the CDR is not locked on both CHA and CHB for this retimer part and no link is established on the SFPs after resetting the device. This part was tested previously and worked as intended with default register setting, except the 0x1F register has to write a bit 1 to invert the outputs on both CHA and CHB. I would like to know if this part needs to be replaced. Please see attached device status screenshots from the SigCon Architect GUI and the register .cfg file if this helps. Any guidance is appreciated. Thanks!