This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP130: Equalizer transfer function parameters

Part Number: SN75DP130


Tool/software:

Hi alll,

Regarding the equalizer,
If the AEQ_L0_LANE0_SET setting in the data sheet is changed as follows,
would it be possible to provide the equalizer transfer function parameters,like pole, zero and gain?

・000 – 0 dB EQ gain (default)
・011 – 4 dB (HBR); 8 dB (HBR2)
・101 – 6 dB (HBR); 13 dB (HBR2)
・111 – 9 dB (HBR); 18 dB (HBR2)

Thanks in advance.
Regards,
Toshi