Tool/software:
Hi TI engineer,
What does "IDLE detect" do? What does "IDLE" state and function?
If an input signal is detected, does it power down or recognize the rate?
Please explain in detail.
Regards,
Shuichi Sugi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi TI engineer,
What does "IDLE detect" do? What does "IDLE" state and function?
If an input signal is detected, does it power down or recognize the rate?
Please explain in detail.
Regards,
Shuichi Sugi
Hi Shuichi-san,
The TXIDLEA/B pins are used to control channel output behavior.
The SD_TH pin is used to adjust the idle detect threshold. Table 7 and Figure 6 in the datasheet explain how to configure this pin. Note that values given in the datasheet are typical, and there is an assert/de-assert hysteresis of the idle detect threshold.
The RATE pin is used to control the pulse width of de-emphasis of the output.
Additionally, TXIDLEA/B, SD_TH, and RATE pin settings can be overridden with register settings if you are using SMBus mode.
Best,
Lucas
Hi Lucas,
Thank you for replying. I understad your explanations.
I have one more question.
Is the definition of an IDLE a setting for pin strap?
In that case, an IDLE state doesn't exist when using SMBUS, right?
Regards,
Shuichi Sugi
Hi Shuichi-san,
Electrical IDLE state simply means the channel output is muted. Electrical IDLE state can be configured with both pin settings and SMBus registers.
Best,
Lucas