Part Number: TMUXHS4212
Tool/software:
I am using TMUX4212 to multiplex PCIe GEN3.0 signals.
Can I multiplex not only data signals but also clock signals with TMUXHS4212?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMUXHS4212
Tool/software:
I am using TMUX4212 to multiplex PCIe GEN3.0 signals.
Can I multiplex not only data signals but also clock signals with TMUXHS4212?
Hi Syuhei,
What voltage are these clock signals? The TMUXHS4212 can support up to 1.8V and 16Gbps, so if the clock signal is within that range, then yes, it can also be used to mux clock signals. Also bear in mind that the TMUXHS4212 cannot support negative voltages, if that is a concern.
Thanks,
Ryan