Part Number: SN65MLVD203
Other Parts Discussed in Thread: SN65MLVD207
Tool/software:
Dear Specialists,
My customer is considering SN65MLVD203 and has questions.
I would be grateful if you could advise.
---
Regarding SN65MLVD203
(1) Is there failsafe circuit in the Receiver Input?
(2) LVDS receiver(not MLVDS receiver) has generally has a offset voltage by failsafe circuit, how about SN65MLVD203?
(3) If question (1) and (2) is Yes, when the input pin is shorted, the output should be either H or L depending on the logic before the short and the individual part, is this understanding correct?
I assumed the following,
If, like the LVDS receiver (DS90LV047), there is a built-in fail-safe that is offset 10m to 30mV to the negative side,
I interpreted that the 25mV hysteresis (L → H) would transition near VID = 0V.
(4) Could you please provide the application note of failsafe bias circuit regarding MLVDS receiver.
---
I appreciate your great help in advance.
Best regards,
Shinichi