Tool/software:
Need to know expected minimum and maximum limits values for the driver High Impedance Output Current parameter and if there is anything I should be looking out for when I test the parameter. Please refer to page 4 of the part datasheet ( SN65LBC176A-EP ).
The datasheet says, “See receiver input currents” and the MIN and MAX fields are blank (do not have any values). I need to know the the actual MIN and MAX limits values to support a qualification test.