Part Number: DP83TC811S-Q1
Tool/software:
When using multiples of this PHY in slave mode using RMII, can the 50MHz oscillator be daisy-chained from one PHY to another and then terminate at the MAC, or does each PHY require its own 50MHz oscillator which must also be connected to the MAC? What is the best topology when implementing multiple PHYs on the same board?