Part Number: TMUXHS4212
Other Parts Discussed in Thread: TS3USB31, HD3SS6126
Tool/software:
Hi, I need to provide USB ports that can be switched off in HW for security reasons. We have previously used USB 2.0 ports with a TS3USB31 to achieve this. I am now swapping to USB 3.2. I cannot find an equivalent USB 3 1:1 switch, but have found several USB 3 mux devices like the TMUXHS4212, which I can leave with one side open (I am only using USB A ports, not C, so do not need to reverse the connections).
Can the TMUXHS4212 be used with the USB 2.0 data signals as well as the USB 3.x signals? Some mux's are explicit that they can be, but this does not mention it.
It would allow me to reduce the number of different parts on my board, and lowers the risk of obsolescence.
Thanks.