This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848T: Strap for RX_ER and Auto-MDIX

Genius 17995 points

Part Number: DP83848T

Tool/software:

Hello

 

My customer has a question for DP83848.

 

They found that RX_EN pin voltage is intermediate voltage around 1.06V due to the internal pull-down of the processor.

Since this pin is a strap pin for MDIX_EN, it means Auto-MDIX could be enabled or disabled right after start up.

They want to enable Auto-MDIX.

They have already released this board. Then they are investigating if it is OK for their product or not.

 

After the start-up, the processor set bit12 and bit 9 to “1” in BMCR register for auto-negotiation restart.

Does this enabling auto-negotiation include enabling Auto-MDIX?

Meaning, even if the Auto-MDIX is disabled by the strap, does enabling auto-negotiation enable Auto-MDIX?

 

Regards,

Oba