This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XIO2001: Malfunction when using an external arbiter

Part Number: XIO2001

Tool/software:

Hi,

We are using the XIO2001 in a new device currently under development, but we are encountering a problem that is delaying our evaluation process.

■ Issue Description
We are experiencing an issue when using the XIO2001 with an external PCI arbiter:
- The device is recognized as a PCIe device during startup.
- However, the BIOS process halts (POST stops) while attempting to configure the PCI side.
- This issue has been confirmed with the PCI target disconnected.
- When using the internal arbiter, the system boots normally (also confirmed with the target disconnected).
- We have disconnected REQ/GNT in hardware and applied pull-up processing to rule out any external arbiter issues.
- Despite this, switching back to the external arbiter does not resolve the POST halt.


■Question
1. Do you have any insights into the cause of this issue or recommendations for a solution?
If there are any similar past cases or known issues, please provide details.

2. We are switching between the internal and external arbiter using the EXT_ARB_EN pin (H/L).
- Are there any other settings required, such as specific register configurations?
- If so, please provide the necessary details.
(*Note: We understand that the REQ/GNT connections differ depending on the arbiter mode.)

3. If there are any application notes or documentation related to the use of the external arbiter with the XIO2001, we would appreciate it if you could share them.

Best regards,

Conor

  • Hello Conor,

    Thank you for reaching out about this observation.

    1. We are aware of Errata #5 in the XIO2001 Errata document, though your observation does not appear to exactly match this errata.
      • Which power rail is being used to pull up EXT_ARB_EN? The EXT_ARB_EN pin will only be sampled when GRST# is de-asserted.
    2. I am not aware of any register settings which are required. You've noted that you are aware of the REQ# / GNT# connections which differ depending on the arbiter mode. Are the un-used REQ# pins on the XIO2001 pulled up to the clamping rail (VCCP) as recommended by data sheet Section 9.2.1.2.1?
    3. The only documents that I am aware of with details on this description are the XIO2001 Implementation Guide and device data sheet.

    Could you help me to better understand the use of the external arbiter in your system vs. the internal arbiter of the XIO2001?

    Best,
    David

  • Hi David,

    Which power rail is being used to pull up EXT_ARB_EN? The EXT_ARB_EN pin will only be sampled when GRST# is de-asserted.

    GRST# is open (PU not implemented), and I am expecting an internal PU. I expect it to be sampled when the power is turned on.

    Extracted from the table on Datasheet P14 Miscellaneous Pins (continued)

    Note: The GRST input buffer has both hysteresis and an internal active pullup. The pullup is active at all times.

    CLAMP RAIL: VDD_33_COMBIO

    Are there any problems with this connection?

    I am not aware of any register settings which are required. You've noted that you are aware of the REQ# / GNT# connections which differ depending on the arbiter mode. Are the un-used REQ# pins on the XIO2001 pulled up to the clamping rail (VCCP) as recommended by data sheet Section 9.2.1.2.1?

    We have recognized that the operation may be affected by the clamp rail (VCCP, PCIR) that should be on the secondary (PCI) side. We will continue to check.

    Could you help me to better understand the use of the external arbiter in your system vs. the internal arbiter of the XIO2001?

    The product uses an external arbiter (because 7-master support is required).
    Operation checks with the internal arbiter were conducted solely for research purposes, to confirm the impact of the arbiter.

    Thanks,

    Conor

  • Hello Conor,

    GRST# is open (PU not implemented), and I am expecting an internal PU. I expect it to be sampled when the power is turned on.

    Extracted from the table on Datasheet P14 Miscellaneous Pins (continued)

    Note: The GRST input buffer has both hysteresis and an internal active pullup. The pullup is active at all times.

    CLAMP RAIL: VDD_33_COMBIO

    If I am understanding you correctly, EXT_ARB_EN is clamped by VDD_33_COMBIO. Is this correct?

    If this is the case, what I am thinking could be happening is that EXT_ARB_EN is rising at the same time as GRST#, which may be causing the pin to be sampled incorrectly when GRST# is de-asserted. I would recommend pulling EXT_ARB_EN up using the VDD_33 power rail, if this is not the case already.

    The product uses an external arbiter (because 7-master support is required).

    Thank you for confirming.

    1. Could you please help to share the schematic of your implementation to help us to better understand the XIO2001's configuration in your system? You can share this here, or over E2E private message if you'd prefer.
    2. Could you share a waveform of your power-up sequence showing VDD_33, VDD_15, PCIR, and GRST#?

    Please note that with the upcoming US holidays, I will be out of the office starting tomorrow and returning on December 30. So, responses will be delayed for a period of time. Apologies for any inconvenience.

    Best,
    David

  • Hi David,

    Our investigation revealed that the cause of the malfunction was a misinterpretation of the external arbiter.
    In this design, an external arbiter was used to consolidate seven external targets into one to support seven masters.
    In this case, the XIO2001 should have been operated in internal arbiter mode.

    Thank you for your follow!

  • Hi Conor,

    Thank you for confirming the resolution of this issue. I'm glad you were able to resolve it Slight smile

    Best,
    David