Part Number: TCAN2451-Q1
Tool/software:
Hi team,
May I know that the following unused pins should be kept floating or connected to GND? Cheers. Thanks.
WAKE1-2 -WAKE2-1, WAKE3-32 WAKE4-31
HSS1-7,HSS2-6,HSS3-5,HSS4-4
CFG-22,
Regards,
Ivy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN2451-Q1
Tool/software:
Hi team,
May I know that the following unused pins should be kept floating or connected to GND? Cheers. Thanks.
WAKE1-2 -WAKE2-1, WAKE3-32 WAKE4-31
HSS1-7,HSS2-6,HSS3-5,HSS4-4
CFG-22,
Regards,
Ivy
Hi Ivy,
WAKE1 through WAKE4 if unused should be disabled and connected to ground - by default they are enabled so you will have to write 0x00 to register address 0x2A (WAKE_PIN_CONFIG3) to shut them off.
HSS1 - HSS4 can be left floating and they should disabled in the software - however they are disabled by default so just don't turn them on if unused.
Pin 22 is GFO - there is no CFG pin on this device; the GFO pin is a general purpose output and can be left floating if unused.
Please let me know if you have any other questions.
Best,
Parker Dodson