This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03001CISQ/NOPB_LVPECL Standard Output Pin Compatibility

Part Number: LMK03001CISQ

Tool/software:

Hello,

For clock conditioner part LMK03001CISQ/NOPB, there are following LVPECL standard compatible Output pins

Does these Output pins support LVPECL standard only or Differential 2.5-V SSTL Class I standard also? Please clarify

  • Shiva,

    This device supports just the standard LVPECL format - any of the termination methods below can be employed:

    The output voltage swing is between 660mV and 965mV. My understanding is that this specification requires a swing between 0.3V and VCC - 0.6V, which this device meets. To be safe, can you provide the specification?

    Thanks,

    Kadeem