Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC814S-Q1: EMI Issue

Part Number: DP83TC814S-Q1

Tool/software:

Hello TI Team,

Now we have the EMI issue in GPS band.

We can know the issue caused by the RGMII TX_CLK and RX_CLK (25MHz).

Do you have any suggestions for improvements via software configuration or hardware?

Best Regards!

Wang Jingkun

  • Hi Jingkun,

    For SW, follow the configurations mentioned in section 3 of this app note: https://www.ti.com/lit/an/snla389b/snla389b.pdf?ts=1734372676088 and program register=0x000F and register=0x0003 to disable switching on 25MHz clkout pin.

    How were you able to find that the source of the issue is RGMII TX_CLK and RX_CLK (25MHz)?

    Best regards,

    Melissa

  • Hi Melissa,

    In the SNLA389B section 3, the software configuration is in order to shorter linkup time.

    We had disabled the 25MHz clkout pin:  

    Reg<0x045F> = 0x000F

    Reg<0x0453> = 0x0003

    How were you able to find that the source of the issue is RGMII TX_CLK and RX_CLK (25MHz)?

    We did some countermeasures on TX_CLK and RX_CLK line, the test result can pass. But it has the loss packets issue after implementing the countermeasures.

    In the SNLA389B section 8,   I can't find the highlighted in the document. 

    Could you tell me which configurations are good for EMI.

    Best Regards!

    Wang Jingkun

  • Hi Jingkun,

    Did disabling the CLKOUT pin help?

    How were you able to find that the source of the issue is RGMII TX_CLK and RX_CLK (25MHz)?

    We did some countermeasures on TX_CLK and RX_CLK line, the test result can pass. But it has the loss packets issue after implementing the countermeasures.

    What is the test setup diagram and picture of the EMI test you are conducting? Do you have a test name or standard?

    In the SNLA389B section 8,   I can't find the highlighted in the document. 

    Could you tell me which configurations are good for EMI.

    Please use all the register configurations mentioned in section 3 of the app note. These configurations are the ones we used to qualify the DP83TC813 for EMC compliance aswell.

    Best regards,

    Melikssa

  • Hello Melissa,

    How were you able to find that the source of the issue is RGMII TX_CLK and RX_CLK (25MHz)?

    --->Above test result is already disable CLKOUT.

    Please use all the register configurations mentioned in section 3 of the app note. These configurations are the ones we used to qualify the DP83TC813 for EMC compliance aswell.

    --->We had used the latest driver.

    // SPDX-License-Identifier: GPL-2.0
    /* Driver for the Texas Instruments DP83TC812 PHY
     * Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/
     */
    /* 01/17/2024 Alvaro Reyes (a-reyes1@ti.com)
    * Updated Open Alliance script for the 812 in both Master and Slave
    * Added SQI, TDR, and Forced-Master/Slave features
     * 
     * 02/08/2024 Alvaro Reyes (a-reyes1@ti.com)
     * 
     * New Global Variables
     * 
     * Updated Functions:
     * dp83812_reset
     * dp83812_phy_reset
     * dp83812_chip_init
     * dp83812_config_init
     * dp83812_config_aned
     * dp83812_probe
     */
    
    #include <linux/ethtool.h>
    #include <linux/ethtool_netlink.h>
    #include <linux/etherdevice.h>
    #include <linux/kernel.h>
    #include <linux/mii.h>
    #include <linux/mdio.h>
    #include <linux/module.h>
    #include <linux/of.h>
    #include <linux/phy.h>
    #include <linux/netdevice.h>
    
    
    #define DP83TC812_CS2_0_PHY_ID			0x2000a271
    #define DP83TC813_CS2_0_PHY_ID			0x2000a211
    #define DP83TC814_CS2_0_PHY_ID			0x2000a261
    
    #define MMD1F							0x1f
    #define MMD1							0x1
    
    #define DP83TC812_STRAP					0x45d
    #define MII_DP83TC812_SGMII_CTRL		0x608
    #define SGMII_CONFIG_VAL				0x027B
    #define MII_DP83TC812_RGMII_CTRL		0x600
    #define MII_DP83TC812_INT_STAT1			0x12
    #define MII_DP83TC812_INT_STAT2			0x13
    #define MII_DP83TC812_INT_STAT3			0x18
    #define MII_DP83TC812_RESET_CTRL		0x1f
    #define MMD1_PMA_CTRL_2					0x1834
    #define DP83TC812_TDR_CFG5				0x0306
    #define DP83TC812_CDCR					0x1E
    #define TDR_DONE						BIT(1)
    #define TDR_FAIL						BIT(0)
    #define DP83TC812_TDR_TC1				0x310
    #define DP83TC812_TDR_START_BIT			BIT(15)	
    #define DP83TC812_TDR_half_open_det_en 	BIT(4)
    #define BRK_MS_CFG						BIT(14)
    #define HALF_OPEN_DETECT				BIT(8)
    #define PEAK_DETECT						BIT(7)
    #define PEAK_SIGN						BIT(6)
    
    #define DP83TC812_HW_RESET				BIT(15)
    #define DP83TC812_SW_RESET				BIT(14)
    
    /* INT_STAT1 bits */
    #define DP83TC812_RX_ERR_CNT_HALF_FULL_INT_EN	BIT(0)
    #define DP83TC812_TX_ERR_CNT_HALF_FULL_INT_EN	BIT(1)
    #define DP83TC812_MS_TRAIN_DONE_INT_EN			BIT(2)
    #define DP83TC812_ESD_EVENT_INT_EN				BIT(3)
    #define DP83TC812_LINK_STAT_INT_EN				BIT(5)
    #define DP83TC812_ENERGY_DET_INT_EN				BIT(6)
    #define DP83TC812_LINK_QUAL_INT_EN				BIT(7)
    
    /* INT_STAT2 bits */
    #define DP83TC812_JABBER_INT_EN			BIT(0)
    #define DP83TC812_POL_INT_EN			BIT(1)
    #define DP83TC812_SLEEP_MODE_INT_EN		BIT(2)
    #define DP83TC812_OVERTEMP_INT_EN		BIT(3)
    #define DP83TC812_FIFO_INT_EN			BIT(4)
    #define DP83TC812_PAGE_RXD_INT_EN		BIT(5)
    #define DP83TC812_OVERVOLTAGE_INT_EN	BIT(6)
    #define DP83TC812_UNDERVOLTAGE_INT_EN	BIT(7)
    
    /* INT_STAT3 bits */
    #define DP83TC812_LPS_INT_EN			BIT(0)
    #define DP83TC812_WUP_INT_EN			BIT(1)
    #define DP83TC812_WAKE_REQ_INT_EN		BIT(2)
    #define DP83TC811_NO_FRAME_INT_EN		BIT(3)
    #define DP83TC811_POR_DONE_INT_EN		BIT(4)
    #define DP83TC812_SLEEP_FAIL_INT_EN		BIT(5)
    
    /* RGMII_CTRL bits */
    #define DP83TC812_RGMII_EN				BIT(3)
    
    /* SGMII CTRL bits */
    #define DP83TC812_SGMII_AUTO_NEG_EN		BIT(0)
    #define DP83TC812_SGMII_EN				BIT(9)
    
    /* Strap bits */
    #define DP83TC812_MASTER_MODE			BIT(9)
    #define DP83TC812_RGMII_IS_EN			BIT(7)
    
    /* RGMII ID CTRL */
    #define DP83TC812_RGMII_ID_CTRL			0x602
    #define DP83TC812_RX_CLK_SHIFT			BIT(1)
    #define DP83TC812_TX_CLK_SHIFT			BIT(0)
    
    /*SQI Status bits*/
    #define DP83TC812_dsp_reg_71			0x871
    #define MAX_SQI_VALUE					0x7
    
    enum DP83TC812_chip_type {
    	DP83TC812_CS1 = 0,
    	DP83TC812_CS2,
    	DP83TC813_CS2,
    	DP83TC814_CS2,
    };
    
    struct DP83TC812_init_reg {
    	int	reg;
    	int	val;
    };
    
    static const struct DP83TC812_init_reg DP83TC812_master_cs2_0_init[] = {
    	{0x001F, 0x8000},
    	{0x0523, 0x0001},
    	{0x0834, 0xC001},
    	{0x081C, 0x0FE2},
    	{0x0872, 0x0300},
    	{0x0879, 0x0F00},
    	{0x0806, 0x2952},
    	{0x0807, 0x3361},
    	{0x0808, 0x3D7B},
    	{0x083E, 0x045F},
    	{0x0834, 0x8000},
    	{0x0862, 0x00E8},
    	{0x0896, 0x32CB},
    	{0x003E, 0x0009},
    	{0x001F, 0x4000},
    	{0x0523, 0x0000},
    };
    
    static const struct DP83TC812_init_reg DP83TC812_slave_cs2_0_init[] = {
    	{0x001F, 0x8000},
    	{0x0523, 0x0001},
    	{0x0834, 0x8001},
    	{0x0873, 0x0821},
    	{0x0896, 0x22FF},
    	{0x089E, 0x0000},
    	{0x001F, 0x4000},
    	{0x0523, 0x0000},
    };
    
    static const struct DP83TC812_init_reg DP83TC812_tdr_config_init[] = {
    	{0x523, 0x0001},
    	{0x827, 0x4800},
    	{0x301, 0x1701},
    	{0x303, 0x023D},
    	{0x305, 0x0015},
    	{0x306, 0x001A},
    	{0x01f, 0x4000},
    	{0x523, 0x0000},
    	{0x01f, 0x0000},
    };
    
    struct DP83TC812_private {
    	int chip;
    	bool is_master;
    	bool is_rgmii;
    	bool is_sgmii;
    };
    
    static int DP83TC812_read_straps(struct phy_device *phydev)
    {
    	struct DP83TC812_private *DP83TC812 = phydev->priv;
    	int strap;
    
    	strap = phy_read_mmd(phydev, MMD1F, DP83TC812_STRAP);
    	if (strap < 0)
    		return strap;
    
    	if (strap & DP83TC812_MASTER_MODE)
    		DP83TC812->is_master = true;
    
    	if (strap & DP83TC812_RGMII_IS_EN)
    		DP83TC812->is_rgmii = true;
    	return 0;
    };
    
    static int DP83TC812_reset(struct phy_device *phydev, bool hw_reset)
    {
    	int ret;
    
    	if (hw_reset)
    		ret = phy_write_mmd(phydev, MMD1F, MII_DP83TC812_RESET_CTRL,
    				DP83TC812_HW_RESET);
    	else
    		ret = phy_write_mmd(phydev, MMD1F, MII_DP83TC812_RESET_CTRL,
    				DP83TC812_SW_RESET);
    
    	if (ret)
    		return ret;
    
    	mdelay(100);
    
    	return 0;
    }
    
    static int DP83TC812_phy_reset(struct phy_device *phydev)
    {
    	int err;
    	int ret;
    
    	err = phy_write_mmd(phydev, MMD1F, MII_DP83TC812_RESET_CTRL, DP83TC812_HW_RESET);
    	if (err < 0)
    		return err;
    
    	ret = DP83TC812_read_straps(phydev);
    	if (ret)
    		return ret;
    
    	return 0;
    }
    
    static int DP83TC812_write_seq(struct phy_device *phydev, const struct
    				DP83TC812_init_reg *init_data, int size)
    {
    	int ret;
    	int i;
    
    	for (i = 0; i < size; i++) {
    		ret = phy_write_mmd(phydev, MMD1F, init_data[i].reg,
    					init_data[i].val);
    		if (ret)
    			return ret;
    	}
    	return 0;
    }
    
    static int DP83TC812_setup_master_slave(struct phy_device *phydev)
    {	
    	switch(phydev->master_slave_set)
    	{
    		case MASTER_SLAVE_CFG_MASTER_FORCE:
    		case MASTER_SLAVE_CFG_MASTER_PREFERRED:
    			return phy_write_mmd(phydev, MMD1, 0x0834, 0xC001);
    		case MASTER_SLAVE_CFG_SLAVE_FORCE:
    		case MASTER_SLAVE_CFG_SLAVE_PREFERRED:
    			return phy_write_mmd(phydev, MMD1, 0x0834,0x8001);
    	case MASTER_SLAVE_CFG_UNKNOWN:
    	case MASTER_SLAVE_CFG_UNSUPPORTED:	
    	default:
    		return 0;	
    	}
    }
    
    static int DP83TC812_read_master_slave(struct phy_device *phydev)
    {
    	int ctrl2 = phy_read_mmd(phydev, MMD1, MMD1_PMA_CTRL_2);
    
    	if (ctrl2 < 0)
    		return ctrl2;
    	
    	if (ctrl2 & BRK_MS_CFG){
    		phydev->master_slave_get = MASTER_SLAVE_CFG_MASTER_FORCE;
    		phydev->master_slave_state = MASTER_SLAVE_STATE_MASTER;
    		return 1;
    	} else {
    		phydev->master_slave_get = MASTER_SLAVE_CFG_SLAVE_FORCE;
    		phydev->master_slave_state = MASTER_SLAVE_STATE_SLAVE;
    		return 0;
    	}
    
    	return 0;
    }
    
    static int DP83TC812_read_status(struct phy_device *phydev)
    {
    	int ret;
    
    	ret = genphy_read_status(phydev);
    	if (ret)
    		return ret;
    	
    	ret = DP83TC812_read_master_slave(phydev);
    	
    	return 0;
    }
    
    static int DP83TC812_sqi(struct phy_device *phydev){
    	int sqi;
    
    	sqi = phy_read_mmd(phydev,MMD1F,DP83TC812_dsp_reg_71);
    
    	if(sqi < 0){
    		printk("Error: Invalid Value.\n");
    		return sqi;
    	}
    
    	sqi = (sqi >> 1) & 0x7;
    
    	return sqi;
    }
    
    static int DP83TC812_sqi_max(struct phy_device *phydev){
    	return MAX_SQI_VALUE;
    }
    
    static int DP83TC812_cable_test_start(struct phy_device *phydev){
    	
    	if(DP83TC812_read_master_slave(phydev)) 
    		printk("PHY is set as Master.\n");
    	else
    		printk("PHY is set as Slave.\n");
    	
    	DP83TC812_write_seq(phydev, DP83TC812_tdr_config_init, ARRAY_SIZE(DP83TC812_tdr_config_init));
    
    	phy_write_mmd(phydev,MMD1F,DP83TC812_CDCR, DP83TC812_TDR_START_BIT);
    
    	msleep(100);
    
    	return 0;
    }
    
    static int DP83TC812_cable_test_report_trans(u32 result) {
    	int length_of_fault;
    	if (result == 0) {
    		printk("No Fault Detected. \n");
    		return ETHTOOL_A_CABLE_RESULT_CODE_OK;
    	} 
    	else if (result & PEAK_DETECT) {
    		length_of_fault = (result & 0x3F);
    
    		// If Cable is Open
    		if(result & PEAK_SIGN){	
    
    			/*if(result & HALF_OPEN_DETECT){
    				printk("Half Open Cable Detected\n");
    				printk("Length of Fault: %d Meters\n",length_of_fault);
    				return ETHTOOL_A_CABLE_RESULT_CODE_OPEN;
    			} */				
    			printk("Open Cable Detected\n");
    			printk("Length of Fault: %d Meters\n",length_of_fault);
    			return ETHTOOL_A_CABLE_RESULT_CODE_OPEN;
    		}
    		// Else it is Short
    		printk("Short Detected\n");
    		printk("Length of Fault: %d Meters\n",length_of_fault);
    		return ETHTOOL_A_CABLE_RESULT_CODE_SAME_SHORT;
    
    	}
    
    	return ETHTOOL_A_CABLE_RESULT_CODE_UNSPEC;
    }
    
    
    static int DP83TC812_cable_test_report(struct phy_device *phydev){
    
    	int ret;
    	ret = phy_read_mmd(phydev,MMD1F,DP83TC812_TDR_TC1);
    	
    	if (ret < 0)
    		return ret;
    	ethnl_cable_test_result(phydev,ETHTOOL_A_CABLE_PAIR_A,DP83TC812_cable_test_report_trans(ret));
    	
    	return 0;
    }
    
    static int DP83TC812_cable_test_get_status(struct phy_device *phydev, bool *finished){
    	int statusReg;
    	int TDR_Done;
    	int TDR_Fail;
    	*finished = false;
    	statusReg = phy_read_mmd(phydev, MMD1F,DP83TC812_CDCR);
    	
    	TDR_Done = statusReg & TDR_DONE;
    	TDR_Fail = statusReg & TDR_FAIL;
    
    	if(TDR_Done && !TDR_Fail){
    		*finished = true;
    		printk("\nTDR HAS COMPLETED AND PASSED\n");
    		return DP83TC812_cable_test_report(phydev);
    	}
    	else if (TDR_Fail){
    		printk("\nTDR HAS FAILED\n");
    	}
    	
    	return -EINVAL;
    }
    
    static int DP83TC812_chip_init(struct phy_device *phydev)
    {
    	struct DP83TC812_private *DP83TC812 = phydev->priv;
    	int ret;
    
    	ret = DP83TC812_reset(phydev, true);
    	if (ret)
    		return ret;
    
    	phydev->autoneg = AUTONEG_DISABLE;
    	phydev->speed = SPEED_100;
    	phydev->duplex = DUPLEX_FULL;
    	linkmode_set_bit(ETHTOOL_LINK_MODE_100baseT_Full_BIT,
    		 phydev->supported);
    	
    	if (DP83TC812->is_master)
    		ret = phy_write_mmd(phydev, MMD1, 0x0834, 0xc001);
    	else
    		ret = phy_write_mmd(phydev, MMD1, 0x0834, 0x8001);
    
    	switch (DP83TC812->chip) {
    	case DP83TC812_CS2:
    		if (DP83TC812->is_master)
    			{
    				ret = DP83TC812_write_seq(phydev,
    						DP83TC812_master_cs2_0_init,
    						ARRAY_SIZE(DP83TC812_master_cs2_0_init));
    				phy_set_bits_mmd(phydev, MMD1F, 0x018B, BIT(6)); //Enables Autonomous Mode
    			}
    		else
    			{
    				ret = DP83TC812_write_seq(phydev,
    						DP83TC812_slave_cs2_0_init,
    						ARRAY_SIZE(DP83TC812_slave_cs2_0_init));
    				phy_set_bits_mmd(phydev, MMD1F, 0x018B, BIT(6)); //Enables Autonomous Mode
    			}
    	break;
    	case DP83TC813_CS2:
    		if (DP83TC812->is_master)
    			{
    				ret = DP83TC812_write_seq(phydev,
    						DP83TC812_master_cs2_0_init,
    						ARRAY_SIZE(DP83TC812_master_cs2_0_init));
    				phy_set_bits_mmd(phydev, MMD1F, 0x018B, BIT(6)); //Enables Autonomous Mode
    			}
    		else
    			{
    				ret = DP83TC812_write_seq(phydev,
    						DP83TC812_slave_cs2_0_init,
    						ARRAY_SIZE(DP83TC812_slave_cs2_0_init));
    				phy_set_bits_mmd(phydev, MMD1F, 0x018B, BIT(6)); //Enables Autonomous Mode
    			}
    	break;
    	case DP83TC814_CS2:
    		if (DP83TC812->is_master)
    			{
    				ret = DP83TC812_write_seq(phydev,
    						DP83TC812_master_cs2_0_init,
    						ARRAY_SIZE(DP83TC812_master_cs2_0_init));
    				phy_set_bits_mmd(phydev, MMD1F, 0x018B, BIT(6)); //Enables Autonomous Mode
    			}
    		else
    			{
    				ret = DP83TC812_write_seq(phydev,
    						DP83TC812_slave_cs2_0_init,
    						ARRAY_SIZE(DP83TC812_slave_cs2_0_init));
    				phy_set_bits_mmd(phydev, MMD1F, 0x018B, BIT(6)); //Enables Autonomous Mode
    			}
    	break;
    	default:
    		return -EINVAL;
    	};
    
    	if (ret)
    		return ret;
    
    	mdelay(10);
    	// phy_write_mmd(phydev, DP83TC812_DEVADDR, 0x523, 0x00);
    	/* Do a soft reset to restart the PHY with updated values */
    	return DP83TC812_reset(phydev, false);
    }
    
    static int DP83TC812_config_init(struct phy_device *phydev)
    {
    	struct device *dev = &phydev->mdio.dev;
    	s32 rx_int_delay;
    	s32 tx_int_delay;
    	int rgmii_delay;
    	int value, ret;
    
    	ret = DP83TC812_chip_init(phydev);
    	if (ret)
    		return ret;
    
    	if (phy_interface_is_rgmii(phydev)) {
    		rx_int_delay = phy_get_internal_delay(phydev, dev, NULL, 0,
    						      true);
    
    		if (rx_int_delay <= 0)
    			rgmii_delay = 0;
    		else
    			rgmii_delay = DP83TC812_RX_CLK_SHIFT;
    
    		tx_int_delay = phy_get_internal_delay(phydev, dev, NULL, 0,
    						      false);
    		if (tx_int_delay <= 0)
    			rgmii_delay &= ~DP83TC812_TX_CLK_SHIFT;
    		else
    			rgmii_delay |= DP83TC812_TX_CLK_SHIFT;
    
    		if (rgmii_delay) {
    			ret = phy_set_bits_mmd(phydev, MMD1,
    					       DP83TC812_RGMII_ID_CTRL,
    					       rgmii_delay);
    			if (ret)
    				return ret;
    		}
    	}
    
    	if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
    		value = phy_read(phydev, MII_DP83TC812_SGMII_CTRL);
    		ret = phy_write_mmd(phydev, MMD1F, MII_DP83TC812_SGMII_CTRL,
    				SGMII_CONFIG_VAL);
    	if (ret < 0)
    		return ret;
    	}
    
    	return 0;
    }
    
    static int DP83TC812_ack_interrupt(struct phy_device *phydev)
    {
    	int err;
    
    	err = phy_read(phydev, MII_DP83TC812_INT_STAT1);
    	if (err < 0)
    		return err;
    
    	err = phy_read(phydev, MII_DP83TC812_INT_STAT2);
    	if (err < 0)
    		return err;
    
    	err = phy_read(phydev, MII_DP83TC812_INT_STAT3);
    	if (err < 0)
    		return err;
    
    	return 0;
    }
    
    static int DP83TC812_config_intr(struct phy_device *phydev)
    {
    	int misr_status, err;
    
    	if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
    		misr_status = phy_read(phydev, MII_DP83TC812_INT_STAT1);
    		if (misr_status < 0)
    			return misr_status;
    
    		misr_status |= (DP83TC812_ESD_EVENT_INT_EN |
    				DP83TC812_LINK_STAT_INT_EN |
    				DP83TC812_ENERGY_DET_INT_EN |
    				DP83TC812_LINK_QUAL_INT_EN);
    
    		err = phy_write(phydev, MII_DP83TC812_INT_STAT1, misr_status);
    		if (err < 0)
    			return err;
    
    		misr_status = phy_read(phydev, MII_DP83TC812_INT_STAT2);
    		if (misr_status < 0)
    			return misr_status;
    
    		misr_status |= (DP83TC812_SLEEP_MODE_INT_EN |
    				DP83TC812_OVERTEMP_INT_EN |
    				DP83TC812_OVERVOLTAGE_INT_EN |
    				DP83TC812_UNDERVOLTAGE_INT_EN);
    
    		err = phy_write(phydev, MII_DP83TC812_INT_STAT2, misr_status);
    		if (err < 0)
    			return err;
    
    		misr_status = phy_read(phydev, MII_DP83TC812_INT_STAT3);
    		if (misr_status < 0)
    			return misr_status;
    
    		misr_status |= (DP83TC812_LPS_INT_EN |
    				DP83TC812_WAKE_REQ_INT_EN |
    				DP83TC811_NO_FRAME_INT_EN |
    				DP83TC811_POR_DONE_INT_EN);
    
    		err = phy_write(phydev, MII_DP83TC812_INT_STAT3, misr_status);
    
    	} else {
    		err = phy_write(phydev, MII_DP83TC812_INT_STAT1, 0);
    		if (err < 0)
    			return err;
    
    		err = phy_write(phydev, MII_DP83TC812_INT_STAT2, 0);
    		if (err < 0)
    			return err;
    
    		err = phy_write(phydev, MII_DP83TC812_INT_STAT3, 0);
    	}
    
    	return err;
    }
    
    #if 0
    static irqreturn_t DP83TC812_handle_interrupt(struct phy_device *phydev)
    {
    	bool trigger_machine = false;
    	int irq_status;
    
    	/* The INT_STAT registers 1, 2 and 3 are holding the interrupt status
    	 * in the upper half (15:8), while the lower half (7:0) is used for
    	 * controlling the interrupt enable state of those individual interrupt
    	 * sources. To determine the possible interrupt sources, just read the
    	 * INT_STAT* register and use it directly to know which interrupts have
    	 * been enabled previously or not.
    	 */
    	irq_status = phy_read(phydev, MII_DP83TC812_INT_STAT1);
    	if (irq_status < 0) {
    		phy_error(phydev);
    		return IRQ_NONE;
    	}
    	if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
    		trigger_machine = true;
    
    	irq_status = phy_read(phydev, MII_DP83TC812_INT_STAT2);
    	if (irq_status < 0) {
    		phy_error(phydev);
    		return IRQ_NONE;
    	}
    	if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
    		trigger_machine = true;
    
    	irq_status = phy_read(phydev, MII_DP83TC812_INT_STAT3);
    	if (irq_status < 0) {
    		phy_error(phydev);
    		return IRQ_NONE;
    	}
    	if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
    		trigger_machine = true;
    
    	if (!trigger_machine)
    		return IRQ_NONE;
    
    	phy_trigger_machine(phydev);
    
    	return IRQ_HANDLED;
    }
    #endif
    
    static int DP83TC812_config_aneg(struct phy_device *phydev)
    {
    	bool changed = false;
    	int err, value, ret;
    
    	if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
    		value = phy_read(phydev, MII_DP83TC812_SGMII_CTRL);
    		ret = phy_write_mmd(phydev, MMD1F, MII_DP83TC812_SGMII_CTRL,
    				SGMII_CONFIG_VAL);
    		if (ret < 0)
    			return ret;
    	}
    
    	err = DP83TC812_setup_master_slave(phydev);
    	if (err < 0)
    		return err;
    	else if (err)
    		changed = true;
    	
    	if (AUTONEG_ENABLE != phydev->autoneg)
    		return genphy_setup_forced(phydev);
    	
    	return genphy_config_aneg(phydev);
    }
    
    static int DP83TC812_probe(struct phy_device *phydev)
    {
    	struct DP83TC812_private *DP83TC812;
    	int ret;
    
    	DP83TC812 = devm_kzalloc(&phydev->mdio.dev, sizeof(*DP83TC812), GFP_KERNEL);
    	if (!DP83TC812)
    		return -ENOMEM;
    
    	phydev->priv = DP83TC812;					
    	ret = DP83TC812_read_straps(phydev);
    	if (ret)
    		return ret;
    
    	switch (phydev->phy_id) {
    	case DP83TC812_CS2_0_PHY_ID:
    		DP83TC812->chip = DP83TC812_CS2;
    	break;
    	case DP83TC813_CS2_0_PHY_ID:
    		DP83TC812->chip = DP83TC813_CS2;
    		break;
    	case DP83TC814_CS2_0_PHY_ID:
    		DP83TC812->chip = DP83TC814_CS2;
    	break;
    	default:
    	return -EINVAL;
    	};
    
    	return DP83TC812_config_init(phydev);
    }
    
    #define DP83TC812_PHY_DRIVER(_id, _name)				\
    	{							\
    		PHY_ID_MATCH_EXACT(_id),			\
    		.name           = (_name),			\
    		.probe          = DP83TC812_probe,		\
    		/* PHY_BASIC_FEATURES */			\
    		.soft_reset     = DP83TC812_phy_reset,		\
    		.config_init    = DP83TC812_config_init,		\
    		.config_aneg = DP83TC812_config_aneg,		\
    		.ack_interrupt = DP83TC812_ack_interrupt,		\
    /*if 0								\
    		.handle_interrupt = dp83812_handle_interrupt,	\
    #endif	*/									\
    		.config_intr = DP83TC812_config_intr,		\
    		.suspend = genphy_suspend,			\
    		.resume = genphy_resume,			\
    		.get_sqi = DP83TC812_sqi,				\
    		.get_sqi_max = DP83TC812_sqi_max,		\
    		.cable_test_start = DP83TC812_cable_test_start, \
    		.cable_test_get_status = DP83TC812_cable_test_get_status, \
    		.read_status	= DP83TC812_read_status,		\
    	}
    
    static struct phy_driver DP83TC812_driver[] = {
    	DP83TC812_PHY_DRIVER(DP83TC812_CS2_0_PHY_ID, "TI DP83TC812CS2.0"),
    	DP83TC812_PHY_DRIVER(DP83TC813_CS2_0_PHY_ID, "TI DP83TC813CS2.0"),
    	DP83TC812_PHY_DRIVER(DP83TC814_CS2_0_PHY_ID, "TI DP83TC814CS2.0"),
    	};
    
    module_phy_driver(DP83TC812_driver);
    
    static struct mdio_device_id __maybe_unused DP83TC812_tbl[] = {
    	// { PHY_ID_MATCH_EXACT(DP83TC812_CS1_0_PHY_ID) },
    	{ PHY_ID_MATCH_EXACT(DP83TC812_CS2_0_PHY_ID) },
    	{ PHY_ID_MATCH_EXACT(DP83TC813_CS2_0_PHY_ID) },
    	{ PHY_ID_MATCH_EXACT(DP83TC814_CS2_0_PHY_ID) },
    	{ },
    };
    MODULE_DEVICE_TABLE(mdio, DP83TC812_tbl);									   
    
    MODULE_DESCRIPTION("Texas Instruments DP83TC812 PHY driver");
    MODULE_AUTHOR("Hari Nagalla <hnagalla@ti.com");
    MODULE_LICENSE("GPL");
    

    What is the test setup diagram and picture of the EMI test you are conducting? Do you have a test name or standard?

    Standard:  FMC1278   RE310

    Best Regards!

    Wang Jingkun

  • Hi Jingkun,

    Do you have a Field Applications Engineer from Texas Instruments? Can you provide the name? I want to see if we are able to move this thread over email. 

    Best regards,

    Melissa

  • Hi Melissa

    Below is supporting our company's  TI FAE.

    Best Regards!

    Wang Jingkun

  • Hi Jingkun,

    Thank you, I recorded the email and deleted it from your message.  Can you provide your email aswell?

    Best regards,

    Melissa

  • Hi  Melissa,

    My e-mail is 

    jingkun.wang@forvia.com

    Best Regards!

    Wang Jingkun

  • Hi Jingkun,

    I am reaching out to you over email and going to close this thread for now.

    Best regards,

    Melissa