Tool/software:
Hello experts
Hope this finds you well.
I am trying to change the SCL_CTL and SDA_CTL pins I2C for SN75DP130SSRGZ.
We think: If you change bit 7 of Offset 05h from 0 to 1 and change bit 4:3 value of Offset 15h, Preemphasis will change by 10%
The waveform changes as we want, but even if I change the EQ setting between Offset 05h and 0Ch, there was no change in waveform.
(If you change the bit 4:3 of 15h, you can see a change in the waveform, so I think that it is successfully accessed to I2C and write the value properly, but the EQ setting does not change.)
I looked at HBR1 and HBR2, and I didn’t feel any change in both.

I looked at this page and it says that Link training is disabled, but when Link training is disabled, it stopped and did not show anything even when the monitor is connected
Is there a procedure to turn Link training back on at the end?
Regards,
Jieyu