Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD72: RS485 Wake Up from Sleep

Part Number: SN65HVD72
Other Parts Discussed in Thread: MAX3223

Tool/software:

In general, it seems these RS485-to-UART converters have a standby/shutdown mode with low current BUT only when the device is fully disabled. This is great for my battery powered application, except how do I know it's time to turn it back on? Is there a standard external "sniffer" type circuit that can monitor the data on the lines and then trigger an interrupt on my MCU to tell it to enable the RS485 again?

I have a RS232-to-UART (MAX3223) that has an auto-powerdown that can detect when data is incoming and turn back on. Is there a solution that achieves similar results for RS485?

  • RS-485 is usually used for industrial application where power usage is not a large concern.

    It might be possible to read the bus voltages with comparators, but when you need to support the entire bus voltage range, this would be hard to do, especially with less than 0.6 mA. Also, the receiver enable time of up to 8 µs might be too long.

  • Hi Michael,

    Below I have highlighted the time required for the device to turn on from the low power mode:

    For instance, if both receiver/driver are disabled, then turning on the driver or receiver takes around 3 us (9us maximum). 

    We currently do not have an RS-485 device that automatically powers on based on incoming data.

    Regards,

    Ethan