Part Number: TCAN1048AV-Q1
Tool/software:
hi expert
i saw the following words in our data.

could you further explain that in which situation 1048 can run in 2,5,8Mbps? like how long wire is? two communication points or multi-points ? .etc
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1048AV-Q1
Tool/software:
hi expert
i saw the following words in our data.

could you further explain that in which situation 1048 can run in 2,5,8Mbps? like how long wire is? two communication points or multi-points ? .etc
thanks
Hi Jay,
Please refer to this thread.
Regards,
Sean
hi Sean
thanks for your quick reply.
i saw the following words in that thread what you mention:
"Note that 8Mbps in only possible in very small and simple networks. Similarly, 5Mbps is difficult to achieve in most real systems."
i think it is too rough. do we build or test 8M or 5M communication system? if yes, can you share details about this system.
thansk
Hi Jay,
Whether can reach a specific data rate or not is a system level question, TI does not build or test a system, all the boards we build (like a EVM) and test are only on the ECU level. Thus, customers need to test in their own system to get the most accurate result.
To be a little bit more specific, 8Mbps is only theoretical maximum the chip can support, but not in a real application. It may be possible in a simple node to node network, with PCB board carefully designed, CMC required. 5Mbps is possible but difficult to realize in real system, the network need to be ideal, no impedance mismatch on board & cabling. For this reason, CAN SIC is highly recommended if customer want 5Mbps communication which can save them a lot of efforts on designing the system.
Regards,
Sean