Part Number: TFP401
Other Parts Discussed in Thread: SN65LVDS93B, DS90C387A,
Tool/software:
Hi everyone,
I have an issue I’d like to clarify. Due to the temperature constraints (my requirement is that the components must operate between -40°C and 80°C), I cannot follow the SALL325 document that explains how to bridge DVI to LVDS for a higher resolution (1920x1200).
Instead, my idea is to use two SN65LVDS93B chips rather than a single DS90C387A. My question is: would this approach work?
Here’s my reasoning:
- I would connect the even pixels from the TFP401 to the first SN65LVDS93B.
- I would connect the odd pixels from the TFP401 to the second SN65LVDS93B.
- Both SN65LVDS93B chips would share the same ODCK, HSYNC, VSYNC, and DE signals.
Could anyone confirm if this setup is viable?
Thank you in advance for your help!
Best regards,