Part Number: DS90UB941AS-Q1
Tool/software:
Hi Team.
The customer plans to use DS90UB941ASRTDTQ1 and DS90UB948TNKDRQ1 to realize the display and control function from host to LCD screen;
Please help to confirm whether it is feasible to adopt the following scheme at the LCD screen side:
1. use pin 45 and pin 46 of DS90UB948TNKDRQ1 chip to connect two other IIC devices (light sensor, backlight power diagnostic) for data reading at the same time;
2. using the DS90UB948TNKDRQ1 chip's pin 16, pin 17, pin 18 to connect to the SPI port of the LCD screen to read the fault diagnostic information of the LCD screen;
3. using the DS90UB948TNKDRQ1 chip pin 8 to control the LCD screen backlight power supply PWM pin, control frequency 10KHZ;
Thanks.