Other Parts Discussed in Thread: TFP401A-EP, TFP401
Hopefully there is someone from the factory who has knowledge of the TFP401A-EP visiting here.
Upon review of the datasheet and other associated information from TI some questions have come up regarding the TFP401A-EP.
- Does anyone know what the clock to out timing specification is for the image output bus (QE[ ], QO[ ], VSYNC, etc.) relative to the output clock (ODCK)? I presume that this varies depending upon output drive strength? I presume it is the same regardless the clock edge (rising or falling) used to clock out the image bus? For some reason the datasheet specifies setup and hold. I am used to setup and hold timing specifications being used for inputs and not for outputs.
- Does anyone know if EXT_RES requires anything? Some of the information suggests leave it unconnected as there already is an internal termination matching circuit within the part. Other information suggests connecting it up to something, what that something is, is not specified. For example resistor size, pull-up, or pull-down.
- Does anyone know if RSVD is supposed to be tied directly to the supply rail or if pulling-up to the supply rail is acceptable. There is only mention of tying it to the supply rail. If it is to be pulled-up, what values are acceptible?
- Does anyone know if it is preferable to pull-up or pull-down the STAG# input when the part is to operate in single pixel mode?
TIA!
Regards,
Carlton