Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD1420: Replace competitor

Part Number: THVD1420

Tool/software:

Hi team,
Please help to recommend suitable devices (P2P would be better) to replace SGM3752YTN6G. The datasheet of competitor as below. Thanks.

TWGMC-MAX485ESA-SOP8-TWGMC.pdf

Best Regards,

Ryker

  • Hi Ryker,

    The best P2P device to replace the MAX485ESA is the THVD1420DR (12Mbps) or THVD1520DR (10Mbps). THVD1400DR could also work but the main difference is that it only supports up to 500kbps. Note that the THVD14XX series supports either 3.3V or 5V supply. 

    Regards,

    Ethan