Part Number: TMDS1204
Tool/software:
I am evaluating the board like this jumper, HDMI2.1 can not recognize, but HDMI2.0 can recognize
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDS1204
Tool/software:
I am evaluating the board like this jumper, HDMI2.1 can not recognize, but HDMI2.0 can recognize
I am using an evaluation board of TMDS120 4, with one end connected to a 2-meter cable and the other end connected to a 0.5-meter cable. The HDMI 2.1 cable can recognize 8k 60HZ normally
Hi,
The evaluation board itself has two HDMI receptacles, and we will need to make sure to use a cable as short as possible to minimize the insertion and return loss from the two receptacles. The one we used is this at this link.
Are you using I2C or pin strap mode to configure TMDS1204? Can you please share your current TMDS1204 configuration either in I2C or pin strap mode?
Thanks
David