This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD8F003: parameter for help

Part Number: TPD8F003

Tool/software:

Hi team

one of my customer wants to replace IP4254CZ16 by TPD8F003, but some parameter is missing in the datasheet.

Could you please help this list, many thanks for you!

TPD8F003

Vrwm—Reverse Stand-Off voltage

VCC---should be Vio(0-5.5V)

Max=5.5V

Pch---Channel power dissipation

Ptot---Total power dissipation

Tstag:  -65—150度

-65~150℃

ILR---Reverse leakage current

10nA

Vf---forward voltage

 

  • Hi Jerry, 

    The only additional spec I can give you is the Reverse stand off voltage is 5.5V. This device is over 15 years old, so I am not sure if power dissipation or channel power dissipation was a parameter that was tested and we don't have any information on it. 

    Best,

    McKenzie