Other Parts Discussed in Thread: LMH0051
Hi Team,
I am assisting a customer who is using one our SVA parts. The customer is using a LMH0051 Deserializer with an SD SDI Input. A clock of 27 MHz and 20 bits of data at 54 MHz is received from the LMH0051. If this is its correct function are ten of the bits valid bits?
It is my understanding that register 28H can be changed to modify the clock and data frequencies. When the clock frequency is lowered by a factor of two (Address 28 bit 6 is set to 0), the Data frequency still remains 54 MHz. Does modifying this register only change the clock frequency?
The customer took o-scope shots of the data and clk.
Cyan: Clock
Magenta: Data
This waveform shows the clock operating at 27 MHz.
This waveform shows the clock operating at 13.5 MHz.
Is there a place where I can find additional support on this device or devices like this one? Any help is greatly appreciated.
Thanks,
Jacob O.