Part Number: THVD1406
Tool/software:
Hi Team,
Please help to review the design of SPI to RS485
Whether this setting can enable two-way data transmission

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THVD1406
Tool/software:
Hi Team,
Please help to review the design of SPI to RS485
Whether this setting can enable two-way data transmission

Hi Clemens,
The RE and SHDN design of THVD1406DR can realize tow-way data transmission.
Yes, but half duplex. On a shared bus, only one device can transmit at the same time.
How should the RE and SHDN pins be programmed if shutdown mode is not required (this device is used in auto-orientation applications).
Hi Allen,
As Clemens pointed out, this schematic looks like it's for UART implementation.
The THVD1406 looks like its set up correctly.
The device has auto-direction control so it is set up for a half duplex implementation has Clemens pointed out.
-Bobby