Tool/software:
Hello, while working with DSLVDS1047-1048EVM, when it's connected to a STM32, one of the components is shortened (U2 - DSLVDS1047PWR) and is needed to be replaced,
it happened more then 3 times on different boards.
Is it related to current limit of the P.S? (I worked with 3.3V / 1A) and the SW seems to run correctly through the component (until it gets malfunctioned).
Thanks!!