Part Number: TMDS181
Other Parts Discussed in Thread: TCA9517
Tool/software:
Tool/software:
Hi team,
There is an "DDC read failed" when TMDS181 at SRC configuration. From customer schematic, this circuit can be configured as SNK side and SRC side.

The sch: HDMI Re-timer 线路12.24.pdf
Test summary:
- Attach R740/R744, configured as SNK, the device work well.
- Detach R740/R744 and attach R741/R745, configured as SRC (but I checked with customer, the pull up resistor R411/R408 is detached, which is different with datasheet figure.32). the product shows DDC read failed.
- Then detach R741/R745 and attach R740/R744 to set to SNK again, still shown DDC read failed issue.
- Replace a new TMDS181 and attach R740/R744, configured as SNK, the device work well.
Questions and support need:
1) According to test 3 and 4, it seems that the device is failed after setting to SRC without pull up resistor. Is this pull up resistor the root cause? If it might be, could you please help to explain the reason? If not, could you please help to provide some suggestions or any potential reason for this issue?
2) Except the pull up resistor, is there any other circuit need be modified in this schematic when change from SNK to SRC?
3) How to fix the board which failed in test 2? Do you have any insights?
I will keep following the debug progress and post to you when there is any update. Thanks!
BRs,
Rannie