Part Number: TLK106
Tool/software:
A few questions:
1. What magnetics are required to work with the TLK106?
2. Is there any version of RJ45 with magnetics that has a breakout board that would work with the TLK106 for some benchtop testing?
3. Do you know if the sparkfun RJ45 with magnetics would work? http://www.sparkfun.com/datasheets/Prototyping/MagJack.pdf (SparkFun RJ45 MagJack Breakout BOB-1302)
4. Why do magnetics allow an ethernet interface to function?
5. Can you use AC coupling instead? https://www.ti.com/lit/an/snla088a/snla088a.pdf?ts=1693325757331&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FDP83848-EP
a. is there a length concern?
b. why would you need ac coupling on each end of the cable? or just one?