Other Parts Discussed in Thread: TUSB9261, TUSB9260
Hi,
In the datasheet for the TUSB9261, page 17, states:
6.3 Oscillator
XI should be tied to the 1.8-V clock source and XO should be left floating.
VSSOSC should be connected to the PCB ground plane.
A 20-, 25-, 30- or 40-MHz clock can be used.
In the implementation guide, the oscillator diagram on page 10 shows Vcc of the oscillator connected to +3.3VDC.
Where does the +1.8VDC comes from in the datasheet?
Is it an artifact from the TUSB9260, which required +3.3V, +1.8V, and +1.1V?
Is the datasheet or the implementation guide correct?
Thanks,
--Bill