Part Number: DS280DF810
Tool/software:
Hi Ti Team,
We are using the DS280DF810ABVT on our card to mux/demux the eCPRI interface to two different QSFP28 connectors. Please find the attached block diagram for your reference. The QSFP28 uses a CAUI-4 C2M interface.
We understand that the inter-pair (pair-to-pair) length matching requirement is determined by the processor and the QSFP28 module, Kindly confirm this. As per the datasheet, DS280DF810ABVT introduces a maximum channel-to-channel inter-pair skew of less than 30 ps.
However, we would like to confirm or clarify the specific length matching requirements for the QSFP28 (CAUI-4 C2M) when used through a DS280DF810ABVT IC
1. Is inter-pair (pair-to-pair) length matching required for the CAUI-4 C2M interface type?
2. Please let us know any additional details that need to be taken care on the layout of DS280DF810
Your insights on this matter will be greatly appreciated. Please let us know if additional details are required.
Looking forward to your response.
Regards,
Gireesh