Part Number: TCAN844-Q1
Other Parts Discussed in Thread: TCAN844V-Q1
Tool/software:
Hi Expert,
VDIFF is -120mV ~+12mV for TCAN844V-Q1. What’s the advantage compared to HVDA551, which is -12mV ~+12mV?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN844-Q1
Other Parts Discussed in Thread: TCAN844V-Q1
Tool/software:
Hi Expert,
VDIFF is -120mV ~+12mV for TCAN844V-Q1. What’s the advantage compared to HVDA551, which is -12mV ~+12mV?
Hi Sean,
Customer needs Environmental Operation Temperature. Dwight gave below reply. Can you help calculate the Ta temperature range?
Hi Beida,
We don't specify an operation ambient temperature in datasheet. The junction temperature is the critical factor in determining the operation of the device. As Dwight said they need to look at table 5.5 thermal characteristics that shows the junction-to-ambient thermal resistance to calculate the maximum junction temperature it can reach at a certain ambient temperature. For example, operating the device at 150C ambient temperature may mean that the junction temperature is above 150C, potentially leading to thermal shutdown.
https://www.ti.com/lit/an/spra953d/spra953d.pdf
Regards,
Sean