Part Number: TUSB4041I
Tool/software:
Hello, I'm trying to choose the capacitors. To choose the capactor value, should I consider DC vias capacitance value?
Some capactor values are written on "10.1 TUSB4041 Power Supply", "10.2 Downstream Port Power" and "11.1.1 Placement of datasheet".
And I wonder if I should follow the value as they are written or I should consider DC bias capacitance at the voltage.
eg. 1uF for VDD33 power supply, is it better to choose GRM155R61E225KE11D (2.2uF, 1.630uF at 3.3V) instead of GRM155R61E105KA12D (1uF, 0.628uF at 3.3V)?