Part Number: TCA6416A
Other Parts Discussed in Thread: TCA9555
Tool/software:
Hi,
I'm considering adopting the TCA6416ARTWR.
Do all I/O pins have built-in Schmitt triggers?
OR, only SDA/SCL have?
Thanks,
Tatsuya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yamamoto-San,
SDA and SCL of our I2C IO expanders use CMOS inputs with minor hysteresis. The signal is then filtered as required by the I2C specification for 50 ns glitches (only I2C target devices have this and require this).
The Pxx pins can be configured to high-z CMOS inputs. I don't believe they have Schmitt trigger inputs on the IO side.
Regards,
Tyler
Hello Tyler,
Thank you for your answer.
I’m concerned about the rise-up time to Pxx pins when using it as an input pin with a pull-up resistor (47kΩ).
The circuit is shown in text below.
[TCA6416A]<---[Protection resistor in series(1kΩ)]<---[Decoupling capacitor b/w GND(0.1uF)]<---[Pull-up resister b/w 3.3V]<---[Physical switch(Open or GND)]
I think the rise-up time will be on the order of milliseconds.
Will not the TCA6416A fail or go into a fault state even with this millisecond input?
Yamamoto-San,
Rise time on the order of milliseconds is okay.
TCA6416A does not have a fail / fault state. This rise-time is okay.
For example, TCA9555 has internal 100k PU resistors. This device operates just fine with large rise-times. The same is true for the TCA6416A.
Regards,
Tyler