Tool/software:
HI friend,
May I ask if this design proposal is okay?(Including the selection of resistors, capacitors and inductors)
use condition: Iout1(typ)=534mA;Iout1(max)=1780mA;Iout2(typ)=748mA;Iout1(max)=1136mA

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
HI friend,
May I ask if this design proposal is okay?(Including the selection of resistors, capacitors and inductors)
use condition: Iout1(typ)=534mA;Iout1(max)=1780mA;Iout2(typ)=748mA;Iout1(max)=1136mA

Hi Yuming,
Thanks for using E2E.
The schematic looks fine.
Best regards,
Sepp