This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD1450: Can i use 3.3V for the tx/rx signals of the THVD1450?

Part Number: THVD1450

Tool/software:

I'm using the THVD1450 in a custom design and the mcu uses 3.3V CMOS logic. Can i use the THV without issues with this logic level if i connect the THVs VCC pin to 3.3V?