Part Number: DS90UB962-Q1
Other Parts Discussed in Thread: DS90UB935-Q1
Tool/software:
Hello
We have encountered an ESD issue of our automatic parking system ECU, camera;
Issue 1: The combined video screen is blurred while we discharging 6KV/8KV on the metal housing of the surround view camera.

Issue 2: The one side(front, or rear, or left, or right) of the video screen is flicker sometimes while we discharging 6KV/8KV on the metal housing of the surround view camera.
Background:
1. We use DS90UB962-Q1 in the ECU side, and DS90UB935-Q1 in the camera side; and the image sensor of camera is OVT OX03F10;
2. We have another camera with Image sensor OVT OX03F10 + MAX96717F, the housing is also metal, this camera can pass the ESD test up to 8KV contact discharge and 15KV air discharge with status A; so we supposed maybe something are different between TI and MAXIM which affect the ESD test, maybe the hardware design, software protocol?
Could you help to do some analysis and give some advices? Please let me know if you need further details.