Part Number: DP83825I
Tool/software:
Hi Team,
I have a question about the contents of the data sheet(Rev. A).
- 6.6 Timing Requirements
Regarding T4 of POWER-UP TIMING, it says within 50ms from the rise of power supply (VAVDD) to the rise of MDC.
I assume this is a description of the stability time after the power supply rises, but isn't this requirement more than 50ms? (min:50ms)
What is the intention of the rating?
- 6.6 Timing Requirements
Regarding T2 of RESET-TIMING, it is stated within 2ms to the rise of MDC after RESET is released.
Does this mean that the rise time of the next MDC must be within 2 ms after the reset is released? (Does it matter if MDC is input before the reset is released?)
Best Regards,
Masaki Takeuchi