Part Number: THVD1424
Tool/software:
Dear TI support team,
I use your THVD1424 for a New Space MRO Project.
I use it in full-duplex, therefore the satellite customer load will be about 100 Ohms, even 120 Ohms as it is point to point connection, only one receiver is interfaced with it.
I have to describe my interface to the customer. Driver spec gives differential output voltage for a VCC of 5V. My VCC is only 3V3, so what would be the minimal and typical differential output voltage on a 100 Ohms (or 120 Ohms) load resistor ?
Also, how would you calculate the power dissipation in regard of datarate ? I couldn't find any Cpd or any way to calculate it in the datasheet.
I precise that I do not use on-chip termination resistor to avoid further self heating of the component.
I thank you in advance for your support.
Regards,
Cédric