Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TG721R-Q1: Phy capabilities always get none

Part Number: DP83TG721R-Q1

Tool/software:

hi  TI expert,

I following the guide (PDK API Guide) to add a new Ethernet PHY and driver.

However, it seems stuck in ENABLE status due to "caps"

Is there any config or init missing?

Thank you for your assistance.

  • Hi WeiTing,

    Can you please reach out to TDA4AL team on this question. DP83TG721 supports only FD1000 (Full Duplex 1000Mbps) and does NOT support auto-negotiation. They can help add these capabilities.

    Thanks,

    David

  • Hi David,

    Yes, we want to apply FD1000 (Full Duplex 1000Mbps) on our project.

    I had check mii_reg_f Register, the result is same as default(0x0).

    Is there any config that I missing such that the Register is still 0x0?

  • Hi WeiTing,

    Can you please reach out to the TDA4AL team on this, they will be better able to assist.

    DP83TG721 capabilities are shown in register 0x1012. Your software is likely showing capability as "none" because DP83TG720 does not support standard ethernet, as shown in register 0xF.

    Thanks,

    David

  • Hi David,

    Ok, I will reach out to the TDA4AL team.

    And, last question,

    I noticed that the DP83TG720 driver configuration(dp83tg721_cs1_slave_init)(link) is different between Linux and RTOS.

    Can the DP83TG720 driver still be used to bring up the DP83TG721?

  • After bypass check cap at reg(0x0f) & change the data in dp83tg720 driver (dp83tg721_cs1_slave_init), it seems linked.

    However, still cannot ping to the MCU.

    Wrong peripheral type, enter again
    Select peripheral type
    0: CPSW_2G
    
    
    Wrong peripheral type, enter again
    Select peripheral type
    0: CPSW_2G
    
    
    Wrong peripheral type, enter again
    Select peripheral type
    0: CPSW_2G
    
    0
    Select MAC port
    0: ENET_MAC_PORT_1 - RGMII
    0
    EnetBoard_setupPorts: 1 of 1 ports configurations found
    CPU Load: 100%
    Starting lwIP, local interface IP is 192.168.1.200
    EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:0 From 1 To 0
    EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:4 From 1 To 0
    EnetMcm: CPSW_2G on MCU NAVSS
    Mdio_open: MDIO manual mode enabled
    PHY 0 is alive
    Cpsw_openPortLink: Cpsw_openPortLink
    
    EnetPhy_bindDriver: PHY 0: OUI:080028 Model:29 Ver:00 <-> 'Dp83tg720' : OK
    Host MAC address: 64:1c:10:22:72:35
    [LWIPIF_LWIP] Enet LLD netif initialized successfully
    status_callback==UP, local interface IP is 192.168.1.200
    Enet lwIP App: Added Network IP address I/F ti0: 192.168.1.200
    Initializing apps
    UDP server listening on port 5001
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    EnetPhy_enableState: PHY 0: enable
    Dp83tg720_readStraps: PHY 0: Strap register is 0x51C0
    
    Dp83tg720_readStraps: PHY 0: Strap: RGMII Mode enabled
    
    Dp83tg720_readStraps: PHY 0: Strap: RX Clock Shift enabled
    
    Dp83tg720_config: PHY 0: Slave Mode enabled
    
    Dp83tg720_chipInit: PHY 0:Dp83tg720_chipInit
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_chipInit: PHY 0: Applying configuration for DP83TG721 CS1 Slave
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_setMiiMode: PHY 0: RGMII Mode enabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII TX Clock Shift disabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII RX Clock Shift enabled
    
    Dp83tg720_configIntr: PHY 0: Disable interrupts
    
    Dp83tg720_setLoopbackCfg: PHY 0: disable loopback
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_printRegs: PHY 0: BMCR    = 0x0140
    
    Dp83tg720_printRegs: PHY 0: BMSR    = 0x0141
    
    Dp83tg720_printRegs: PHY 0: PHYIDR1 = 0x2000
    
    Dp83tg720_printRegs: PHY 0: PHYIDR2 = 0xa290
    
    Dp83tg720_printRegs: PHY 0: PHY_GIGESR = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYSTS  = 0x0004
    
    Dp83tg720_printRegs: PHY 0: PHYCR   = 0x000b
    
    Dp83tg720_printRegs: PHY 0: MISR1   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: MISR2   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: RECR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: BISCR   = 0x0100
    
    Dp83tg720_printRegs: PHY 0: MISR3   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: REG19   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: CDCR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYRCR  = 0x0000
    
    Dp83tg720_printRegs: PHY 0: SGMII_CTRL = 0x007b
    
    Dp83tg720_printRegs: PHY 0: RGMII_CTRL = 0x0128
    
    Dp83tg720_printRegs: PHY 0: RGMII_DELAY_CTRL = 0x0002
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_CONTROL = 0x8001
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_EXT_CASP = 0x0002
    
    EnetPhy_enableState: PHY 0: req caps: FD1000
    EnetPhy_enableState: PHY 0: PHY caps: FD1000
    EnetPhy_enableState: PHY 0: MAC caps: FD1000 FD100 HD100 FD10 HD10
    EnetPhy_enableState: PHY 0: refined caps: FD1000
    EnetPhy_enableState: PHY 0: PHY is not NWAY-capable
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    EnetPhy_enableState: PHY 0: enable
    Dp83tg720_readStraps: PHY 0: Strap register is 0x51C0
    
    Dp83tg720_readStraps: PHY 0: Strap: RGMII Mode enabled
    
    Dp83tg720_readStraps: PHY 0: Strap: RX Clock Shift enabled
    
    Dp83tg720_config: PHY 0: Slave Mode enabled
    
    Dp83tg720_chipInit: PHY 0:Dp83tg720_chipInit
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_chipInit: PHY 0: Applying configuration for DP83TG721 CS1 Slave
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_setMiiMode: PHY 0: RGMII Mode enabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII TX Clock Shift disabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII RX Clock Shift enabled
    
    Dp83tg720_configIntr: PHY 0: Disable interrupts
    
    Dp83tg720_setLoopbackCfg: PHY 0: disable loopback
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_printRegs: PHY 0: BMCR    = 0x0140
    
    Dp83tg720_printRegs: PHY 0: BMSR    = 0x0141
    
    Dp83tg720_printRegs: PHY 0: PHYIDR1 = 0x2000
    
    Dp83tg720_printRegs: PHY 0: PHYIDR2 = 0xa290
    
    Dp83tg720_printRegs: PHY 0: PHY_GIGESR = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYSTS  = 0x0004
    
    Dp83tg720_printRegs: PHY 0: PHYCR   = 0x000b
    
    Dp83tg720_printRegs: PHY 0: MISR1   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: MISR2   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: RECR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: BISCR   = 0x0100
    
    Dp83tg720_printRegs: PHY 0: MISR3   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: REG19   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: CDCR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYRCR  = 0x0000
    
    Dp83tg720_printRegs: PHY 0: SGMII_CTRL = 0x007b
    
    Dp83tg720_printRegs: PHY 0: RGMII_CTRL = 0x0128
    
    Dp83tg720_printRegs: PHY 0: RGMII_DELAY_CTRL = 0x0002
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_CONTROL = 0x8001
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_EXT_CASP = 0x0002
    
    EnetPhy_enableState: PHY 0: req caps: FD1000
    EnetPhy_enableState: PHY 0: PHY caps: FD1000
    EnetPhy_enableState: PHY 0: MAC caps: FD1000 FD100 HD100 FD10 HD10
    EnetPhy_enableState: PHY 0: refined caps: FD1000
    EnetPhy_enableState: PHY 0: PHY is not NWAY-capable
    CPU Load: 3%
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    EnetPhy_enableState: PHY 0: enable
    Dp83tg720_readStraps: PHY 0: Strap register is 0x51C0
    
    Dp83tg720_readStraps: PHY 0: Strap: RGMII Mode enabled
    
    Dp83tg720_readStraps: PHY 0: Strap: RX Clock Shift enabled
    
    Dp83tg720_config: PHY 0: Slave Mode enabled
    
    Dp83tg720_chipInit: PHY 0:Dp83tg720_chipInit
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_chipInit: PHY 0: Applying configuration for DP83TG721 CS1 Slave
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_setMiiMode: PHY 0: RGMII Mode enabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII TX Clock Shift disabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII RX Clock Shift enabled
    
    Dp83tg720_configIntr: PHY 0: Disable interrupts
    
    Dp83tg720_setLoopbackCfg: PHY 0: disable loopback
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_printRegs: PHY 0: BMCR    = 0x0140
    
    Dp83tg720_printRegs: PHY 0: BMSR    = 0x0141
    
    Dp83tg720_printRegs: PHY 0: PHYIDR1 = 0x2000
    
    Dp83tg720_printRegs: PHY 0: PHYIDR2 = 0xa290
    
    Dp83tg720_printRegs: PHY 0: PHY_GIGESR = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYSTS  = 0x0004
    
    Dp83tg720_printRegs: PHY 0: PHYCR   = 0x000b
    
    Dp83tg720_printRegs: PHY 0: MISR1   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: MISR2   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: RECR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: BISCR   = 0x0100
    
    Dp83tg720_printRegs: PHY 0: MISR3   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: REG19   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: CDCR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYRCR  = 0x0000
    
    Dp83tg720_printRegs: PHY 0: SGMII_CTRL = 0x007b
    
    Dp83tg720_printRegs: PHY 0: RGMII_CTRL = 0x0128
    
    Dp83tg720_printRegs: PHY 0: RGMII_DELAY_CTRL = 0x0002
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_CONTROL = 0x8001
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_EXT_CASP = 0x0002
    
    EnetPhy_enableState: PHY 0: req caps: FD1000
    EnetPhy_enableState: PHY 0: PHY caps: FD1000
    EnetPhy_enableState: PHY 0: MAC caps: FD1000 FD100 HD100 FD10 HD10
    EnetPhy_enableState: PHY 0: refined caps: FD1000
    EnetPhy_enableState: PHY 0: PHY is not NWAY-capable
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    EnetPhy_enableState: PHY 0: enable
    Dp83tg720_readStraps: PHY 0: Strap register is 0x51C0
    
    Dp83tg720_readStraps: PHY 0: Strap: RGMII Mode enabled
    
    Dp83tg720_readStraps: PHY 0: Strap: RX Clock Shift enabled
    
    Dp83tg720_config: PHY 0: Slave Mode enabled
    
    Dp83tg720_chipInit: PHY 0:Dp83tg720_chipInit
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_chipInit: PHY 0: Applying configuration for DP83TG721 CS1 Slave
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_setMiiMode: PHY 0: RGMII Mode enabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII TX Clock Shift disabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII RX Clock Shift enabled
    
    Dp83tg720_configIntr: PHY 0: Disable interrupts
    
    Dp83tg720_setLoopbackCfg: PHY 0: disable loopback
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_printRegs: PHY 0: BMCR    = 0x0140
    
    Dp83tg720_printRegs: PHY 0: BMSR    = 0x0141
    
    Dp83tg720_printRegs: PHY 0: PHYIDR1 = 0x2000
    
    Dp83tg720_printRegs: PHY 0: PHYIDR2 = 0xa290
    
    Dp83tg720_printRegs: PHY 0: PHY_GIGESR = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYSTS  = 0x0004
    
    Dp83tg720_printRegs: PHY 0: PHYCR   = 0x000b
    
    Dp83tg720_printRegs: PHY 0: MISR1   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: MISR2   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: RECR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: BISCR   = 0x0100
    
    Dp83tg720_printRegs: PHY 0: MISR3   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: REG19   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: CDCR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYRCR  = 0x0000
    
    Dp83tg720_printRegs: PHY 0: SGMII_CTRL = 0x007b
    
    Dp83tg720_printRegs: PHY 0: RGMII_CTRL = 0x0128
    
    Dp83tg720_printRegs: PHY 0: RGMII_DELAY_CTRL = 0x0002
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_CONTROL = 0x8001
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_EXT_CASP = 0x0002
    
    EnetPhy_enableState: PHY 0: req caps: FD1000
    EnetPhy_enableState: PHY 0: PHY caps: FD1000
    EnetPhy_enableState: PHY 0: MAC caps: FD1000 FD100 HD100 FD10 HD10
    EnetPhy_enableState: PHY 0: refined caps: FD1000
    EnetPhy_enableState: PHY 0: PHY is not NWAY-capable
    CPU Load: 3%
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    EnetPhy_enableState: PHY 0: enable
    Dp83tg720_readStraps: PHY 0: Strap register is 0x51C0
    
    Dp83tg720_readStraps: PHY 0: Strap: RGMII Mode enabled
    
    Dp83tg720_readStraps: PHY 0: Strap: RX Clock Shift enabled
    
    Dp83tg720_config: PHY 0: Slave Mode enabled
    
    Dp83tg720_chipInit: PHY 0:Dp83tg720_chipInit
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_chipInit: PHY 0: Applying configuration for DP83TG721 CS1 Slave
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_setMiiMode: PHY 0: RGMII Mode enabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII TX Clock Shift disabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII RX Clock Shift enabled
    
    Dp83tg720_configIntr: PHY 0: Disable interrupts
    
    Dp83tg720_setLoopbackCfg: PHY 0: disable loopback
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_printRegs: PHY 0: BMCR    = 0x0140
    
    Dp83tg720_printRegs: PHY 0: BMSR    = 0x0141
    
    Dp83tg720_printRegs: PHY 0: PHYIDR1 = 0x2000
    
    Dp83tg720_printRegs: PHY 0: PHYIDR2 = 0xa290
    
    Dp83tg720_printRegs: PHY 0: PHY_GIGESR = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYSTS  = 0x0004
    
    Dp83tg720_printRegs: PHY 0: PHYCR   = 0x000b
    
    Dp83tg720_printRegs: PHY 0: MISR1   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: MISR2   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: RECR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: BISCR   = 0x0100
    
    Dp83tg720_printRegs: PHY 0: MISR3   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: REG19   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: CDCR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYRCR  = 0x0000
    
    Dp83tg720_printRegs: PHY 0: SGMII_CTRL = 0x007b
    
    Dp83tg720_printRegs: PHY 0: RGMII_CTRL = 0x0128
    
    Dp83tg720_printRegs: PHY 0: RGMII_DELAY_CTRL = 0x0002
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_CONTROL = 0x8001
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_EXT_CASP = 0x0002
    
    EnetPhy_enableState: PHY 0: req caps: FD1000
    EnetPhy_enableState: PHY 0: PHY caps: FD1000
    EnetPhy_enableState: PHY 0: MAC caps: FD1000 FD100 HD100 FD10 HD10
    EnetPhy_enableState: PHY 0: refined caps: FD1000
    EnetPhy_enableState: PHY 0: PHY is not NWAY-capable
    Wrong peripheral type, enter again
    Select peripheral type
    0: CPSW_2G
    
    
    Wrong peripheral type, enter again
    Select peripheral type
    0: CPSW_2G
    
    
    Wrong peripheral type, enter again
    Select peripheral type
    0: CPSW_2G
    
    0
    Select MAC port
    0: ENET_MAC_PORT_1 - RGMII
    0
    EnetBoard_setupPorts: 1 of 1 ports configurations found
    CPU Load: 100%
    Starting lwIP, local interface IP is 192.168.1.200
    EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:0 From 1 To 0
    EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:4 From 1 To 0
    EnetMcm: CPSW_2G on MCU NAVSS
    Mdio_open: MDIO manual mode enabled
    PHY 0 is alive
    Cpsw_openPortLink: Cpsw_openPortLink
    
    EnetPhy_bindDriver: PHY 0: OUI:080028 Model:29 Ver:00 <-> 'Dp83tg720' : OK
    Host MAC address: 64:1c:10:22:72:35
    [LWIPIF_LWIP] Enet LLD netif initialized successfully
    status_callback==UP, local interface IP is 192.168.1.200
    Enet lwIP App: Added Network IP address I/F ti0: 192.168.1.200
    Initializing apps
    UDP server listening on port 5001
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    EnetPhy_enableState: PHY 0: enable
    Dp83tg720_readStraps: PHY 0: Strap register is 0x51C0
    
    Dp83tg720_readStraps: PHY 0: Strap: RGMII Mode enabled
    
    Dp83tg720_readStraps: PHY 0: Strap: RX Clock Shift enabled
    
    Dp83tg720_config: PHY 0: Slave Mode enabled
    
    Dp83tg720_chipInit: PHY 0:Dp83tg720_chipInit
    Dp83tg720_resetHw: PHY 0: global hard-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_chipInit: PHY 0: Applying configuration for DP83TG721 CS1 Slave
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_setMiiMode: PHY 0: RGMII Mode enabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII TX Clock Shift disabled
    
    Dp83tg720_configClkShift: PHY 0: RGMII RX Clock Shift enabled
    
    Dp83tg720_configIntr: PHY 0: Disable interrupts
    
    Dp83tg720_setLoopbackCfg: PHY 0: disable loopback
    
    Dp83tg720_reset: PHY 0: global soft-reset
    
    Dp83tg720_isResetComplete: PHY 0: global reset is  complete
    
    Dp83tg720_printRegs: PHY 0: BMCR    = 0x0140
    
    Dp83tg720_printRegs: PHY 0: BMSR    = 0x0141
    
    Dp83tg720_printRegs: PHY 0: PHYIDR1 = 0x2000
    
    Dp83tg720_printRegs: PHY 0: PHYIDR2 = 0xa290
    
    Dp83tg720_printRegs: PHY 0: PHY_GIGESR = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYSTS  = 0x0084
    
    Dp83tg720_printRegs: PHY 0: PHYCR   = 0x000b
    
    Dp83tg720_printRegs: PHY 0: MISR1   = 0x4400
    
    Dp83tg720_printRegs: PHY 0: MISR2   = 0x0000
    
    Dp83tg720_printRegs: PHY 0: RECR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: BISCR   = 0x0100
    
    Dp83tg720_printRegs: PHY 0: MISR3   = 0x0800
    
    Dp83tg720_printRegs: PHY 0: REG19   = 0x0400
    
    Dp83tg720_printRegs: PHY 0: CDCR    = 0x0000
    
    Dp83tg720_printRegs: PHY 0: PHYRCR  = 0x0000
    
    Dp83tg720_printRegs: PHY 0: SGMII_CTRL = 0x007b
    
    Dp83tg720_printRegs: PHY 0: RGMII_CTRL = 0x0128
    
    Dp83tg720_printRegs: PHY 0: RGMII_DELAY_CTRL = 0x0002
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_CONTROL = 0x8001
    
    Dp83tg720_printRegs: PHY 0: MMD1_PMA_PMD_EXT_CASP = 0x0002
    
    EnetPhy_enableState: PHY 0: req caps: FD1000
    EnetPhy_enableState: PHY 0: PHY caps: FD1000
    EnetPhy_enableState: PHY 0: MAC caps: FD1000 FD100 HD100 FD10 HD10
    EnetPhy_enableState: PHY 0: refined caps: FD1000
    EnetPhy_enableState: PHY 0: PHY is not NWAY-capable
    Cpsw_handleLinkUp: Port 1: Link up: 1-Gbps Full-Duplex
    MAC Port 1: link up
    link_callback==UP
    CPU Load: 3%

  • Hi WeiTing,

    Glad to hear the PHY appears linked after bypassing the cap at reg 0xF. Can you read register 0x1 and ensure bit[2] equals 1?

    Which MAC interface are you using? Can you please share the schematic? If link is up but communication is not possible, this generally points to an issue with the MAC interface configuration.

    Thanks,

    David

  • Hi David,

    Can you read register 0x1 and ensure bit[2] equals 1?

    -> Reg 0x01 value is 0x0145 after RTOS indicates phy status is linked.

    -> Additionally, Reg 0x10 value is 0x0605.

    -> Both regs indicate link is up.

    Which MAC interface are you using?

    -> we want to use RGMII interface.

    Can you please share the schematic?

    -> my colleague previously posted the schematic related to the PHY chip. I'm not sure if this is sufficient.

    https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1435171/dp83tg721r-q1-tda4al-q1-ethernet-phy-schematics-review

  • Hi WeiTing,

    Glad to hear that link is up. The MAC interface may be the limiting factor here then. I see RX shift mode is enabled and TX shift mode is disabled. 

    Can you verify on the MAC side that RX shift mode is disabled and TX shift mode is enabled? Below is the required configuration.

    Thanks,

    David

  • Hi David,

    I couldn’t find the MAC side RX/TX shift mode configuration, so I reached out to the TDA4AL team. I’m still waiting for their reply.

    In the meantime, I came across this post(e2e link) about configuring rx/tx shift mode in MAC.

    Following its suggestion, I tried commenting out the code for RGMII TX delay, the result is same as two days ago(phy is linked, but unalbe to ping).

    Additionally, I found another post discussing RX clock configuration.(disscuss about config rx clk) In that post, it was mentioned that the TX/RX clock on the TDA4 side can be configured in the PHY  via RGMII Control Register (RGMIICTL) & Reg addr 0x86 - RGMII Delay Control Register (RGMIIDCTL)

    I’m confused by this statement.

    Does this mean that the RGMIICTL and RGMIIDCTL registers can configure RGMII on the MAC side, and the PHY’s RX/TX clock is configured using GPIOs?

    Looking forward to your clarification.

  • Hi David,

    after struggle a day, I try few couple set about rx/tx shift mode and RTOS MAC side TX/RX shift mode setting.

    Finnally, It's work!!

    Thank you, David.