Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869EVM
Tool/software:
Hi,
I created a 100/1G media converter based of the DP83869EVM. So far I have not gotten it to work.
The first issue I observed is that when I power on the media converter with the fiber and copper connected the link LEDs are OFF. And you do not get 1.8V on the VDDA1P8.
However if I leave the fiber cable disconnected then power on the media converter and finally I plug in the fiber cable. The link LEDs are ON. And you can detect 1.8V on the VDDA1P8.
My understanding of this, correct me if I am wrong, is that the IC is OFF if I don't get 1.8V on VDDA1P8. Its should know that there is only 2 supplies and go into a 2 supply configuration, and the IC will generate 1.8V. Just like in the EVM where it works automatically.
I read on this forum that:
"The PHY will be able to detect the presence/absence of the 1.8V rail supply and be able to go into 2-supply mode vs 3-supply. This is why there is a time limit of 50ms max on VDDA1P8 for rail to ramp."
Please help