This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB981-Q1: Please recommend the appropriate solution according to the application

Part Number: DS90UB981-Q1
Other Parts Discussed in Thread: DS90UB988-Q1

Tool/software:

Please recommend the appropriate solution according to the application

  • Hi Tony,

    For SER/DES solutions, I'll work from the top to the bottom

    • 2880*1620 @60fps
      • PCLK = 279.936MHz
      • No FPD-Link SERs support LVDS at this PCLK
      • The DS90UB988-Q1 DES supports LVDS at this PCLK
    • 2560*1440 @60fps
      • PCLK = 221.184MHz
      • No FPD-Link SERs support LVDS at this PCLK
      • The DS90UB988-Q1 DES supports LVDS at this PCLK
    • Cluster (1920*480 @60fps) / HUD (1920*480 @60fps)
      • PCLK = 55.3MHz per screen
      • For the cluster, a DS90UB927-Q1 SER and DS90UB928-Q1 DES can be used
      • For the HUD, a DS90UB27-Q1 SER and DS90UB928-Q1 DES can be used

    Best,

    Jack