Part Number: TCAN334
Other Parts Discussed in Thread: TCAN3414
Tool/software:
Hello experts,
We are using the TCAN334 (soon we will switch to the TCAN3414) along with the 6432 IWRL radar chip. Our device seems to work robustly alone on a network with just one other receiving node. We have a PCAN adapter that monitors the device's traffic. We have tested this setup extensively and the device works indefinitely. We have a trace file of typical network traffic from a full network populated with other devices. The device handles the network traffic just fine unless the trace is looped and eventually the device enters an error passive state with the ACK error code. I am looking for reasons why our device's messages would stop being ACK'd by the network?
In the above description the only other active device on the network is our PCAN adapter which is handling the trace replaying so this situation is similar to the previous cases we have tested other than the other messages.
One issue I would like to explore with some expert help is if the RX FIFO is full and in blocking mode, does the device stop ACK'ing other messages on the network?
Thank you in advance.