Other Parts Discussed in Thread: DS100MB203
Tool/software:
Hi
We would like to use the SN65LVCP114 on a line card in a chassis switch, with an 10G/GE Ethernet optical port(SFP+) on the line side and Host interface connected to the Active and Standby switch chips respectively. There are a few questions I would like to confirm:
- Does the SN65LVCP114 terminate the timing information for serdes. Can both switch chips recover the clock from the signal at the same time for SyncE function?
- What is the maximum Propagation Variation for the SN65LVCP114 in a 10GE and 1GE interface application?
- If the line side needs to support eight 10GE/GE optical ports, is there a more suitable alternative chip that can be used?
Thanks
Fang Youxiang