Other Parts Discussed in Thread: TCAN1044-Q1
Tool/software:
Hi,
I used the IBIS model of the TCAN1044-Q1 (which is identical to the TCAN1051HGV-1) for signal integrity (SI) simulation. When performing the simulation using the differential pins (6-7), I encounter an error message related to the IBIS model.
As an alternative, I tested the single-ended mode, and I was able to establish communication between the two CAN devices without any issues. However, during the simulation, I observed the correct inverting signal, but with different voltage levels. Specifically, in "Recessive" mode, where CANH is LOW and CANL is HIGH, the voltage is 2.3V instead of the expected 2.5V as specified in the datasheet. Is this normal?

Best Regards,
Pierre