Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS160PR410: signal chain check

Part Number: DS160PR410
Other Parts Discussed in Thread: SN75LVPE3101,

Tool/software:

Hi TIer

When we use the DS160PR410RNQR as the sata redriver, can the signal chain be referenced as follows (replace SN75LVPE3101 with DS160PR410) ?

There have a question in the location of the serial cap in the above diagram. According to the sata protocol specification, the recommended links are as follows, that is, both transmitter and receiver need to have the serial cap . The second half of the typical application of the SN75LVPE3101, which is connected to a SATA device, is also designed in this way.

But HOST is connected to the SN75LVPE3101 with only one serial capacity, what is the reason?