Part Number: TUSB2036
Tool/software:
Hi,
I am encountering a usage problem on PORT 1.
The design uses 3 permanently connected ports:
- PORT 1: Connection to equipment integrating embedded Linux with USB configured as Ethernet via USB (RNDIS).
- PORT 2: USB-Serial connection using a CP2102 circuit which works perfectly.
- PORT 3: Using a Lithium battery charger circuit. USB communication is only used to determine the maximum charging current.
I am currently experiencing a communication problem on PORT 1. The USB connection is detected and the RNDIS driver is loaded but communication is not taking place.
If I disconnect the USB RNDIS from the HUB and connect it directly everything works. It is clear that the problem is with the TUSB2036 HUB.
I am adding my electronic diagram here if you can help me identify the problem.
Thanks in advance,
Best regards,